Technical FAQs

Ask a Question

How do you adjust the minimum speed on an Omepak 8804?

P8 on the control board is the minimum speed adjustment. Full clockwise will adjust the minimum speed to 50% of the maximum speed.


CTA-ID : 4065
Was this helpful?
What can we do to improve the information ?