Technical FAQs

Ask a Question

Why will the Omegapak 8804 drive not run in Hand or Automatic?

For test purpose try to jumper terminals 34 to 44 to see if the drive starts. If it does, problem is in wiring of the H-O-A switch. Suspect wiring problem.

CTA-ID : 4063
Was this helpful?
What can we do to improve the information ?