Technical FAQs

Ask a Question

How can you add a key operated switch for emergency where will have drive run at 100% (full) speed in Emergency position on an Omegapak 8804 System where the drive is controlled by a PLC panel?

In the emergency position, needs 3 contacts blocks. 1) one contact block will close terminals 44 to 34, 2) one contact block will close terminals 2 to 14 and 3) one contact block will open terminals 22 to 78.


CTA-ID : 4061
Was this helpful?
What can we do to improve the information ?