Technical FAQs

Ask a Question

How do you change the DOI display from hertz to % ( percentage ) speed on the Omegapak 8804?

Need to go to MENU 8, select User input scale (#2) and enter 1.67, then got to MENU 8 select user lable (#3) and enter % Speed. Then goto MENU 7 and select item #3 (Save) and select SAVE. This will save the setup.


CTA-ID : 4057
Was this helpful?
What can we do to improve the information ?