Technical FAQs

Ask a Question

What is the drive type F Omegapak 8804?

It is a true variable torque drive for Fan application unlike the type labeled EVT which is the enhanced variable torque unit which had modications to obtain variable torque rating.


CTA-ID : 4055
Was this helpful?
What can we do to improve the information ?