Technical FAQs

Ask a Question

Can an LE36300LI breaker be swapped for an LH in an I-LINE panel?

Issue:
Can an LE36300LI breaker be swapped for an LH in an I-LINE panel?

Product Line:
Panelboard or switchboard with I line distribution.

Environment:
Products made in the United States.

Cause:
Product features.

Resolution:
The LH is 6`` and the LE is 7.5`` mounting height.
Note:  The LE is an obsolete circuit breaker.

CTA-ID : 2825

Was this helpful?
What can we do to improve the information ?