Technical FAQs

Ask a Question

PDCFA2 and the AL100FA. Are these the same?

No. The AL100FA is the std lug on the FA type breaker and the PDCFA2 is a power distribution connector that can be used for multiple load connections to one breaker.


CTA-ID : 2870
Was this helpful?
What can we do to improve the information ?