Technical FAQs

Ask a Question

Does the EHB24070 take up 4 spaces? How about the EHB24080, EHB24090, EHB24100?

Yes, two vertical spaces and two horizontal spaces. Rejection feature prevents mounting breakers directly accross which would cause too much heat.

CTA-ID : 2865
Was this helpful?
What can we do to improve the information ?