Technical FAQs

Ask a Question

What is the number of operations for a circuit breaker?

Issue:
What is the number of operations for a circuit breaker?
 
Product Line:
Legacy Square D Breakers, Powerpact Breakers, Masterpact Breaker
 
Environment:
Panel Mount and Unit Mount Applications
 
Resolution:
UL 489 Endurance Testing
 
Frame Size
Amperes
Full Load
Operations
 
No Load Operations
0–100 6,000 4,000
101–225 4,000 4,000
226–600 1,000 5,000
601–800 500 3,000
801–2500 500 2,000
2501–4000 400 1,100

See catalog, 0601CT9101

CTA-ID : 1964
Was this helpful?
What can we do to improve the information ?