Technical FAQs

Ask a Question

What is the parameter of the 1000-2000 magnetic adjustment for a KAL36200 ?

The numbers are in Amperes. The tolerance is +/- 25% on the 1000A setting and +/- 20% on all other settings.


CTA-ID : 1958
Was this helpful?
What can we do to improve the information ?