Technical FAQs

Ask a Question

Do I need to use the window CT that comes with the GFM100FA, GFM100FI or GFM250?

It is a neutral CT and is provided for use on 4-wire systems only. If there is no neutral, it should be discarded.


CTA-ID : 1673
Was this helpful?
What can we do to improve the information ?