Technical FAQs

Ask a Question

What is the part number for the shaft only for the D10 switches?

There are three to choose from. For enclosure depth of 5 5/8`` - 6`` shaft only is D11SH4, for enclosure depth of 6`` - 10`` shaft only is D11SH10 and for enclosure depth 10`` - 16`` shaft only is D11SH16. These replacement part numbers are not in print.

CTA-ID : 1670
Was this helpful?
What can we do to improve the information ?