Technical FAQs

Ask a Question

What does the F/S indicate on catalog number QO24L70F/S?

This is actually a short cut for listing two separate load center catalog numbers. The F/S indicates the type of cover style included with the loadcenter. A QO24L70F will include a cover suitable for a flush mount application, while the QO24L70S will include a cover suitable for a surface mount application.


CTA-ID : 1657
Was this helpful?
What can we do to improve the information ?