Technical FAQs

Ask a Question

Why is the single pole HOM breaker labeled with a 120/240 Vac rating.

This labeling describes the type of electrical system it is designed for. The single pole breaker does not have a rating for a 240Vac system. The single pole breaker would attach to one phase of a 120/240Vac system which would be 120Vac.


CTA-ID : 1947
Was this helpful?
What can we do to improve the information ?