Technical FAQs

Ask a Question

Does the GFM100FA require a permanent 120V power source or just for testing the ground fault function?

The 120V power is only required to test the module, you can use a temporary power set-up for this test and then remove the temporary 120V.

CTA-ID : 1651
Was this helpful?
What can we do to improve the information ?