Technical FAQs

Ask a Question

When was the TESYS product launched?

The official launch date of the product was May 11, 2001. As of May 31, 2001 all literature is available from the fulfillment center. Included are 2 catalogs, 2 brochures, and a poster. A CD with a selector, CAD drawings (in PDF Format) will be released in July. CAD drawings in DWG format are also available from the technical library of squared.com.


CTA-ID : 1644
Was this helpful?
What can we do to improve the information ?