Technical FAQs

Ask a Question

Are the 8910DPA contactors available with NC contacts? Can the contacts be field converted?

The 8910 DPA contactors cannot be field converted from NO to NC. The 8910`s are not availabld with any NC power poles.

CTA-ID : 1933
Was this helpful?
What can we do to improve the information ?