Technical FAQs

Ask a Question

Are Class 8536 and 8502 enclosed NEMA devices available with DC control coils?

No, however the use of DC control interposing relay used in conjunction with Class 8536 or 8502 devices controlled by line voltage is possible.


CTA-ID : 1926
Was this helpful?
What can we do to improve the information ?