Technical FAQs

Ask a Question

Is a unit-mount enclosure available for the FDL type circuit breaker?

FD, FG, and FJ breakers are available in I-Line construction only. There is no FDL, FGL, or FJL, and no unit-mount enclosure is available.

CTA-ID : 2228
Was this helpful?
What can we do to improve the information ?