Technical FAQs

Ask a Question

Can a 30-Blank QMB switch be modified to a 30-30?

No, the blank unit cannot be converted to a switch. If there are any plans to add circuits later, a 30-30 switch should be used.


CTA-ID : 1900
Was this helpful?
What can we do to improve the information ?