Technical FAQs

Ask a Question

Will the QO I-Line adapter, catalog number HQO206 and HQO306, accept QO GFI/Arc Fault breakers?

Issue:
Will the QO I-Line adapter, catalog number HQO206 and HQO306, accept QO GFI/Arc Fault breakers?\

Product Line:
I-Line panelboards and accessories sold and supported in the USA.

Environment:
Appliation 

Cause:
Installation 

Resolution:
No, the load terminal comes too close to the support brackets that hold the covers in place. 




CTA-ID : 1824
Was this helpful?
What can we do to improve the information ?