Technical FAQs

Ask a Question

What is the part number for a pilot light kit for a Class 8911 starter?

Pilot light kits are not available for the Class 8911 Starters. The only option is for the customer to install a 22mm or 30mm pilot light in the sidewall of the enclosure.

CTA-ID : 2204
Was this helpful?
What can we do to improve the information ?