Technical FAQs

Ask a Question

Cross reference to Square D from ABB type S4N 480V 225A

Crosses to KCL34225 in thermal-mag and to LEL36225LS in electronic trip.
S4N has 40kA AIR at 500Vac. S4N is IEC only. KC and LE are UL


CTA-ID : 1897
Was this helpful?
What can we do to improve the information ?