Technical FAQs

Ask a Question

What is the difference between the HOM816L125C and the HOM816L125TC?

Issue:
Product design features

Product Line:
Homeline load centers

Environment:
product differences

Resolution:
The HOM816L125TC has the ground bar factory installed and for the HOM816L125C you must purchase the PK15GTA separately and field install it.


CTA-ID : 1302
Was this helpful?
What can we do to improve the information ?