Technical FAQs

Ask a Question

Are the AC Power Accessories, catalog numbers SDM4AC and SDM8AC, provided with receptacles installed?

No, the receptacles must be purchased separately and field installed. Use standard duplex receptacles, 20 ampere, 125 volt, 2 wire with ground (NEMA 5-20R). The SDM4AC accepts two receptacles. The SDM8AC accepts four receptacles.


CTA-ID : 2184
Was this helpful?
What can we do to improve the information ?