Technical FAQs

Ask a Question

What does the ``H`` represent on a Class 8536 Type SCH2?

This is the Class 8536 Type SCA2, changing the ``A`` to ``H`` provides NEMA 3R enclosure in place of the NEMA 12 enclosure.


CTA-ID : 1584
Was this helpful?
What can we do to improve the information ?