Technical FAQs

Ask a Question

How does a HOML2200 fit into a branch position of a Homeline loadcenter?

The HOML2200 was the Main Lug Kit used on 150 ampere and 200 ampere Main Lugs Only, Series 1 Homeline loadcenters. It is not a branch mount device. It is not a circuit breaker and does not provide overcurrent protection. It should only be used as a replacement main lugs device in existing Series 1 Homeline loadcenters.

CTA-ID : 1832
Was this helpful?
What can we do to improve the information ?