Technical FAQs

Ask a Question

Can the GFM be reverse fed?

No. If these modules are reverse fed, the continual voltage on the ground fault shunt trip in the breaker and the trip indicator on the module will burn out.


CTA-ID : 1565
Was this helpful?
What can we do to improve the information ?