Technical FAQs

Ask a Question

Is there a maintained start/stop control station for Class 8536 Type S*G devices?

Class 9999 Type SC22 on/off selector switch will provide this function for size 00 through size 4 and Class 9001 Type KS11BH13 with Class 9001 Type KN245 legend plate on size 5 through size 7. Caution should be exercised when using maintained controls as in event of power failure automatic start will occur upon restoration of power.

CTA-ID : 1481
Was this helpful?
What can we do to improve the information ?