Technical FAQs

Ask a Question

What is the Cross-Reference for a Joslyn J9200-9A and J9200-10 Surge Arrester?

The J9200-9A was a 650Vac to Ground maximum, 3-phase surge arrestor. Current equivalent is SDSA3650. The J9200-10 was a 175Vac to Ground maximum, single-phase arrestor. Current equivalent is SDSA1175.


CTA-ID : 1562
Was this helpful?
What can we do to improve the information ?