Technical FAQs

Ask a Question

Is there a 3 pole, 125 ampere branch breaker available for a QO loadcenter?

Issue:
Application

Product Line:
QO LC

Cause:
Application/Selection

Resolution:
The largest 3 pole circuit breaker available for the QO load centers is 100A. For a 125 ampere load, you may want to consider using a QO3125SL Sub-Feed Lug Kit to feed from the loadcenter to a separtedly mounted enclosed circuit breaker. 


CTA-ID : 2156
Was this helpful?
What can we do to improve the information ?