Technical FAQs

Ask a Question

What options are available for a handle padlock attachment for the PAF, PCF, PXF, PEF?

These frames have a handle padlock attachment factory installed as standard.
A ``PL`` suffix on the circuit breaker catalog number will factory install an additional padlock attachment which meets the USERC requirements.


CTA-ID : 2150
Was this helpful?
What can we do to improve the information ?