Technical FAQs

Ask a Question

MHL3630025DC1680-----The MH series of DC trip curve does not have this 300A breaker with a 25DC prefix trip curve. What trip curve should be used?

What determines the correct trip curve to be used is the prefix ``25DC``. The curve to use is number 660-4. This curve is for the LH series of breakers, however, the 25DC mag trip for both breakers will correspond to each other.

CTA-ID : 1823
Was this helpful?
What can we do to improve the information ?