Technical FAQs

Ask a Question

What doe the suffix TF indicate on a sensor such as XSAV01801TF ?

This indicates an extended Temperature Range to -40 Degree F. The sensor has been tested to that operating range. There is no form fit or functional differences between the TF and the standard sensor in normal operating ranges. If the user substitutes a standard sensor for the extended range version, the substitute may or may not work correctly in the extended operating region.


CTA-ID : 1225
Was this helpful?
What can we do to improve the information ?