Technical FAQs

Ask a Question

What amperage of tenant breakers are available for a MPR64200?

Tenant breakers for 200 ampere maximum MP, MPR and MPH Meter-Pak Meter Centers, which accept QOM2____MM or QOM2____MVH tenant breakers, are available in 100, 125, 150, 175 and 200 ampere sizes.

CTA-ID : 1805
Was this helpful?
What can we do to improve the information ?