Technical FAQs

Ask a Question

What is minimum and maximum enclosure depth for 9422 Type R circuit breaker operators?

Listed below are the standard minimum and maximum dimension required. The addition of Class 9422 Type R2 shaft extension will extend the maximum depth 7 additional inches.

Switch Min. Max.
RG1 6.00`` 17.75``
RN1 5.38`` 17.75``
RP1 6.38`` 17.88``
RR1 7.44`` 18.25``
RT1 9.00`` 18.38``
RX1 11.00`` 18.37``



CTA-ID : 1229
Was this helpful?
What can we do to improve the information ?