Technical FAQs

Ask a Question

How can metric threads be included on a 9012GAW5 ? What is the restriction for a Form M12 to G*WM devices per digest 172 p. 20-4 ?

Use a 9012GAWM5 per digest 170 p. 18-12 . Standard metric connections on 9012GAWM: 20mm BSPT4568 G 1/4 BS2779. Form M12 modifies 9012G*WM devices only. It changes the dimensions of the conduit and pressure connections: PG13.5 conduit entry and 1/4 19 BSP pressure connection.


CTA-ID : 1221
Was this helpful?
What can we do to improve the information ?