Technical FAQs

Ask a Question

What is the part number for the interior deadfront trim for a HOM816M150FTRB or a HOM816M200FTRB loadcenter?

Issue:
Current design repair parts

Product Line:
Homeline Load Centers

Environment:

Repair parts

Cause:

Maintenance

Resolution:

The interior deadfront trim part number is dependent upon the Series # of the loadcenter. For Series 1, Series 2 and Series S01, the interior deadfront trim is obsolete and no longer available. For Series S02 or S03, use part number 40563-133-01.

CTA-ID : 1791
Was this helpful?
What can we do to improve the information ?