Technical FAQs

Ask a Question

Are the QO816L100F, S, DF, DS, DFCU, DSCU, RB or RBCU, UL listed as Suitable for Use as Service Equipment (ULSE)?

Issue:
Product design features

Product Line:
QO load centers

Environment;
Service Entrance Rating

Cause:
Application

Resolution:

Yes, under either of two circumstances:
1. With a field-installed back-fed main service disconnect. Retaining Kit PK2MB is required to retain the back-fed main breaker.
2. When not more than six service disconnecting means are provided and when not used as a lighting and appliance branch circuit panelboard, per the National Electrical Code,

CTA-ID : 1506
Was this helpful?
What can we do to improve the information ?