Technical FAQs

Ask a Question

Does the NSJ400 have a lug that will accept 2-3/0 wires per phase?

The 600A lugs, part number 32510, accept 2 wires and will fit on the 400A breakers.
Wire range: 2/0 - 350 kcmil CU; 2/0 - 500 kcmil Al

CTA-ID : 2101
Was this helpful?
What can we do to improve the information ?