Technical FAQs

Ask a Question

Is there a handle lock for Multi 9 supplementary protectors?

The handle padlock for the C60N is MG26970 which is non-UL Listed. For the NC100H the handle padlock is MG27145.


CTA-ID : 2091
Was this helpful?
What can we do to improve the information ?