Technical FAQs

Ask a Question

What mounting socket is used with a standard 9050JCK on delay, interval, or repeat cycle timer, and the 9050JCK60 timer?

Use the eight pin socket, 8501NR51 for single tier and the 8501NR52 for the two tier.

CTA-ID : 1185
Was this helpful?
What can we do to improve the information ?