Technical FAQs

Ask a Question

How does one order a custom legend plate with white lettering on black background and a 30 X 40 mm holder for an XB4 operator ?

Order a ZBY2002 (describe the text , maximum 2 lines with 11 characters). This is a 8 X 27 mm legend insert and 30 X 40 mm holder.

CTA-ID : 1477
Was this helpful?
What can we do to improve the information ?