Technical FAQs

Ask a Question

What are the available control coil voltages for Form R6 with the Class 8903 mechanically held lighting contactors?

For Class 8903 Type L - 24 VAC, 120 VAC, 240 VAC, 277 VAC, and 480 VAC.

For Class 8903 Type S - 24 VAC, 120 VAC, 208 VAC, 240 VAC, 277 VAC, 480 VAC, and 600 VAC. (24V coil is not available for 200 through 800 amp devices)



CTA-ID : 1473
Was this helpful?
What can we do to improve the information ?