Technical FAQs

Ask a Question

Is the Horn Bypass that is installed on the ringless type MPH Meter-Pak metering equipment rated for continuous use?

No, the Horn Bypass is ONLY rated for temporary use. Ekstrom Industries, Inc. manufactures a bypass (Meter Socket Jumper Cover) for continuous use. This company can be reached at 800-532-4332 or 248-477-0250.

CTA-ID : 2370
Was this helpful?
What can we do to improve the information ?