Technical FAQs

Ask a Question

Do all CM UL listed AC voltage shunt trips operate at 55% of voltage?<br />

All CM UL listed AC voltage shunt trips operate at 55% of voltage (75% for DC).
See technical manual (AC0036/3E page 12) for the UL breaker.


CTA-ID : 2372
Was this helpful?
What can we do to improve the information ?