Technical FAQs

Ask a Question

Is the C200RBJ obsolete and was it replaced by the RC200S.

The C200RBJ is obsolete and the RC200S is a replacement device, BUTnot a direct replacement because the C200RBJ is a Ring Type device and the RC200S is Ringless. Need to check with local utility before installing the device.

CTA-ID : 2366
Was this helpful?
What can we do to improve the information ?