Technical FAQs

Ask a Question

How does an 8501XS1 work and can it be tested in the field ?

It limits the spike produced when the relay is deenergized and the coil magnetic field collapses, to approximately 200% of the nominal coil voltage. It is only suitable for use on AC coils up to 120 volts. It is a resistor/capacitor circuit and should have some resistance when tested.


CTA-ID : 1745
Was this helpful?
What can we do to improve the information ?