Technical FAQs

Ask a Question

What is the contact block position layout for a 9001TS6 ?

Looking from the back of the switch, side one is the left and side 2 is the right. Odd positions, 1,3, and 5 or on the left and even positions are on the right. The Type T operators use the same H contact block assembly codes that are used on the Type K and SK.

CTA-ID : 1740
Was this helpful?
What can we do to improve the information ?