Technical FAQs

Ask a Question

What are the repair parts for catalog number QO11224L125GRB, Series S02?

Issue:
Current design repair parts

Product line:
QO Load Centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
RB Cover - 4056317850
Interior trim with Labels - 4056312801K
Interior Assembly - QO11224L125GRBI
Neutral Bonding Hardware - 4028345850K
Main Lugs - QOL125
RB Cover Latch - 4056314701
Latch rivet - 2410212160
interior trim mounting screw - 4020513001K
RB door mounting screws - 2142217101
Main circuit breaker and main lugs keps nut - 2342702001


CTA-ID : 2348
Was this helpful?
What can we do to improve the information ?